Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Transporter Distance Control Crash

Hi

 

when I use this code in a distance control for a transporter Mu then Plant Sim crashes

 

>>>>

 

(distanceIsBelowLimit : boolean)
is
do
    -- Pause if the transporter are in the parking area
    if distanceIsBelowLimit and
       ?.location.~.Name = "ForkliftParking" then
        -- set pause
        ?.pause := true;
    else
        -- reset pause
        ?.pause := false;
    end;
end;

 

<<<<<<

 

I think it is because i use the code in combination with a FlowControl object that are connected with a source.

 

But the iretating part are that Plant crashes, and when it startsup from the recovery file it keeps crashing and I there for loss the model until last saved. See error meessage in the attached file.

 

 

2 REPLIES 2

Re: Transporter Distance Control Crash

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi

 

you are right. There was a crash when using distance control and FlowControl object. This bug already is fixed (12.0.3). Please use the newest version.

 

For the problem when loading the recovery file please load the model or contact GTAC.

 

Kind regards

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Transporter Distance Control Crash

Thanks! That did the trick.