Cancel
Showing results for 
Search instead for 
Did you mean: 

Transporter control

Experimenter
Experimenter

Hello, I have a problem with transporter controling. 

How should it work?
Only two trucks will leave the parking at the beginning. The first truck will go to UNLOAD and the second truck will go to WAITPLACE. When the truck (UNLOAD) finished the unload, another truck (WAITPLACE) gets a sign for arriving to unloading place and at the same time when truck leave waiting place, another truck will leave the Parking.
I have to simulate 24 hours this way. 

I tried to create it but it does not work well.
Can anybody help me with that? 

TransporterControl.jpg

 

4 REPLIES

Re: Transporter control

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have simplified your model; in the init-method I created the first two trucks; if you have no connectors, you dont need to lock and unlock the exits of the blocks and a simple exit control rear triggers the movement of the other trucks

have a look...

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Transporter control

Experimenter
Experimenter

Thank you for your simplification.
But as soon as the truck arrives at the waiting place, the other truck immediately leaves UNLOAD. When I set UNLOAD Processing time for 50 minutes, is it possible for the truck on WAITPLACE to wait until the truck leaves the UNLOAD?

Re: Transporter control

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
it is only a matter of animation, set the eventcontroller to realtime x100; then you can see the waiting of the truck in the waitPlace
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Transporter control

Experimenter
Experimenter

Oh, sorry. Thank you so much.