Cancel
Showing results for 
Search instead for 
Did you mean: 

Trigger2

Hallo

 

 I want to connect basically Trigger in a model. I have German Version of Model so it does not work with 1,.mus.green, const 

I upload a simple model I want to connect trigger in this model 

3 REPLIES 3

Re: Trigger2

Phenom
Phenom

Basically it's the same as in the last posted model.

 

The trigger object in the library was missing, ( how to reload, s. class libraries in help file)

 

Have a look at the attached file.

Re: Trigger2

Hallo

 

Its work but the problem is when model connecting with trigger then methods are not working

the same problem with above model trigger2 

 

Re: Trigger2

Phenom
Phenom

Only the method "method" is set as exit control

 

In the method you are referring to the Mu "Typ_3", which 

 

is not created by the trigger. 

 

Therefore doesn't exist.

 

The trigger creates the Mus "West","Ost","Norden".

 

Please adapt the methods( method/method1)  according to the the created MUs

 

Unbenannt.PNG