Cancel
Showing results for 
Search instead for 
Did you mean: 

Trouble Using Rack Lane

Creator
Creator

How to connect a Rack Lane to a Conveyer. While trying practice model, When connecting a Conveyer to a Rack Lane, it's asking "side entrance" and "main entrance". Can someone differentiate those two.

2 REPLIES 2

Re: Trouble Using Rack Lane

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

both are just different locations from which parts can be fed into your HBW, other than that they don´t differ.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution


Re: Trouble Using Rack Lane

Creator
Creator

Can you exlain a bit in the view of Rack Lane what these two enterances are?  As far i can see, there is only one enterance, call it side enterance or main enterance.