Cancel
Showing results for 
Search instead for 
Did you mean: 

Turntable Rotation Issues

Phenom
Phenom

Hello all

 

We have recently set up a turntable for a project and have found a strange occurrence with 13.1 and was wondering if anyone else has spotted this yet? (Tested in 13 and the issue is not there)

 

When a MU has loaded onto the turntable it will move to a slightly strange angle (around 5 degrees in the wrong direction) and sit there before unloading the part without rotating at all, and then it will rotate back to the correct position ready to take the next MU from the angle it should have unloaded the previous MU at.

 

Simple model attached displaying the error.

 

JamesM

 

1 REPLY 1

Re: Turntable Rotation Issues

Siemens Phenom Siemens Phenom
Siemens Phenom
Hello JamesM, The error you found is an amimation bug in 3D. The simulation results and the animation in 2D are correct. The error will be fixed in the next maintenance pack which is planned for March 17th. Kind regards Karola
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.