Cancel
Showing results for 
Search instead for 
Did you mean: 

Turntable turning more than 1 (2 - n) units at a time

Experimenter
Experimenter

Hi all,

 

I would have a need to turn more than 1 MU at a time with turntable. The help of turntable clearly says "The Turntable has a capacity of one, i.e. only one part can be located on it at any one time."

 

Anyhow, is there a trick, how turning of several items at a time would work?

 

My own idea was creating a container on the turntable, and then moving MUs to be turned on that container. However, it seems that creating a container on turntable with .create is impossible.

 

Thanks for your ideas!

2 REPLIES 2

Re: Turntable turning more than 1 (2 - n) units at a time

Experimenter
Experimenter

For additional explanation, attached is a figure of the required steps.

Re: Turntable turning more than 1 (2 - n) units at a time

Phenom
Phenom

why not load the MUs on to the container

 

before moving on to the turntable..

 

Unbenannt.PNG