Cancel
Showing results for 
Search instead for 
Did you mean: 

Two Interesting details in 12.1

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
  1. I found it a bit odd that method getcolYdim was created but getrowXdim wasn't. Meaning I would need to transpose all tables having data by rows.
  2. Debugger expressions seems to not work properly with formulas as shown in the next picture

debugger expressions.png

 

cortega@interlatin.com.mx
+52 (81) 10801310
InterLatin S de RL de CV
4 REPLIES 4

Re: Two Interesting details in 12.1

Legend
Legend

Yeah, I found the first point odd too. Would make sense to add both.

 

For the second part, is the method formatted as a SimTalk 1.0 method? You need to convert it correctly to a SimTalk 2.0 method to use expressions in 12.1. It's been mentioned to be fixed in the coming patch.

 

So replace local with var, remove ; and remove is do end;.

Then add var before all the variables you had between is and do.

Replace the return value to use -> instead. 

Re: Two Interesting details in 12.1

Siemens Phenom Siemens Phenom
Siemens Phenom

Plant Simulation internally stores the contents of a table in a list of columns. Therefore Plant Simulation can find out the y-dimension of a column very fast. Computing the x-dimension of a row would be significantly slower (in case that there are many columns). I think this is the reason we implemented only 'getColumnYDim'.

If you really need a 'getRowXDim', please say so. We then might provide it in the next version.

 

As has already been said, it is a known bug that in version 12.1 the debugger cannot evaluate some expressions. We will fix this for the next maintenance pack.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Two Interesting details in 12.1

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Actually it was in a V2.0 method.

But the thing is in this case arithmetic formulas cannot be evaluated.

 

Anyway for me where interesting details... if the does't make sense incorporating a getrowXdim for performance reasons then its ok.

 

Good day

cortega@interlatin.com.mx
+52 (81) 10801310
InterLatin S de RL de CV

Re: Two Interesting details in 12.1

Siemens Phenom Siemens Phenom
Siemens Phenom

We are aware that the debugger expression problem exists in SimTalk 1.0 and 2.0. We have already fixed that problem for the next maintenance pack (that will probably be released in about 3 weeks from now).

As a workaround, you can enclose your expression in to_str().

For example the expression '1+2' is not working, but 'to_str(1+2)' is.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.