Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Two Land Track/Track Length

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi all,

 

I have a plant drawing I'm using as the background and specific distances from one area to another. Is there a way to set the distance I want for the track, but have the track look like whatever length I want? For example: it's 600 ft from area A to area B, but when I place the track between those two areas I have a plant Sim length of ~200 ft because the scales are different between the grid and background.

 

Thanks!

1 REPLY 1

Re: Two Land Track/Track Length

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Just kidding! I figured it out. Instead of selecting a start point and end point and having Plant Sim determine the length you can manually enter the length you want then adjust the track accordingly.