Cancel
Showing results for 
Search instead for 
Did you mean: 

Two Portals in the portalcrane

Hi everyone,

i want to know how can i use two portals in the portalcrane. I have one portal that uses a method, but when i insert a second portal some error in the methods start to show up, so how does that work?

- Thanks

1 REPLY 1

Betreff: Two Portals in the portalcrane

Gears Phenom Gears Phenom
Gears Phenom

Are you talking about the "Cranes" library, and if so the "StorageCrane" object or the "MultiPortalCrane" object?

What does your "method" do, what are the errors that show up, can you upload the model with the issue or replicate it in a test model?

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!