Cancel
Showing results for 
Search instead for 
Did you mean: 

Two machines with exitStrategyBlocking connected to a FlowControl

Legend
Legend

Hello,

 

I have found something odd when connecting a source with unlimited capacity with two machines with exitStrategyBlocking to a FlowControl and then to a third SingleProc connected to a Drain.

 

When the two first machines are set to blocking, the statistics displays them as waiting (although the LED is indicating blocking) and when set to not blocking, the behaviour is as expected with blocked status.

 

I've attached a model showing this behaviour. Change the exitStrategyBlocking attribute with the checkbox and see the effects in the chart.

 

Is this intended?

1 REPLY 1

Re: Two machines with exitStrategyBlocking connected to a FlowControl

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Verbalins,

 

this looks like a bug and it must be investigated in more detail.

It seems to be a problem of the statistical evaluation, because the method ResBlocked shows the expected state.

Thank you for the hint.

 

Regards,

Peter