Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Two minor things I've noticed in 12.2

Legend
Legend

Hello,

 

I've noticed two minor things in 12.2.

 

When creating a text box in a dialogue and selecting Data type, the last item there is called "Positve Real Number" instead of "Positive Real Number". The help entry is correct.

 

The icon for the buffer is not consistent with the rest of the objects that share the same look. See the picture below. The first is the current Buffer, the second is the current SingleProc for comparison and the last one is the corrected icon for the Buffer. The current icon lack the white outline at the top.

 

buffer with changes.png

1 REPLY 1

Re: Two minor things I've noticed in 12.2

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Verbalins,

 

thanks for reporting this.

 

We will fix this in the next major version.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.