Cancel
Showing results for 
Search instead for 
Did you mean: 

Undo operations

Experimenter
Experimenter

Hello,

 

How do I undo an operation when I made a mistake in Plant Simulation? Is this possible?

 

Thanks in advance,

Malin

3 REPLIES

Re: Undo operations

Legend
Legend
No, it's only possible to undo mistakes made while writing code in a method or cancel a change before applying it in a dialog. The recommendation is to enable auto saving of the model by starting Plant Simulation with -a XX where XX is the number of minutes between saves.
Highlighted

Re: Undo operations

Experimenter
Experimenter

Okay, thanks. How do I make settings for auto saving?

Re: Undo operations

Legend
Legend
If you have a shortcut to Plant Simulation, you go into the properties of it, and after the path in Target: you add -a 10 for ten minutes between saves.

The target path will look like this for a default installation of Plant Simulation 13.1:
"C:\Program Files\Siemens\Tecnomatix Plant Simulation 13.1\PlantSimulation13_1.exe" -a 10