Cancel
Showing results for 
Search instead for 
Did you mean: 

Unexpected result

Builder
Builder

In my model i was checking the effect of increasing worker on the throughput,and i found out that by increasing number of workers,the throghput decreases.but when i check the stats from Drain it increases when workers becomes 2 and becomes constant with 3 workers.why the xperiment manager showing wrong result? i am attaching a snapshot of xperiment and utilisation of worker.please tell me wts wrong??

1 REPLY 1

Re: Unexpected result

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

difficult to reply. Your results from the experiment manager show, that your output is somewhere between 300 and more than 5000 for one experiment. You should find the reasons for that. May be the duration for the experiments are too short, look at this discussion:

 

http://community.plm.automation.siemens.com/t5/Plant-Simulation-Forum/Warm-up-period-of-a-simulation...

 

Or some experiments are not running until the end and you have jams upstream the drains, you need to find out this. But for sure, something is wrong with your model.

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net