Cancel
Showing results for 
Search instead for 
Did you mean: 

Unplanned % in statistics indicating wrong value

Hi All,

 

I am running my model for 39 days. In which model is running all three shifts with 6 days working. As default it starts from 5th Jan 2015 (Monday) to 13th Feb 2015. In that total 5 sundays come. So statistics must indicate 5/39 = 12.82% but it is showing 13.51% (5.26 days).

 

Please help me to understand from where it is adding the extra 0.69%.

 

Following table indicates the shift timming.

 

Shift NameShift TimingShift Working DaysBreaks
FromTo
Monday
Tuesday
Wednesday
Thrusday
Friday
Saturday
Sunday
Day Shift6:3015:10 YY Y Y6:30-6:35; 9:00-9:08; 11:30-12:00; 13:30-13:37; 15:05-15:10
Afternoon Shift15:1023:50 Y Y Y Y YY N15:10-15:15; 18:00-18:08; 19:45-20:15; 22:00-22:07; 23:45-23:50
Night Shift23:506:30 Y N23:50-23:55; 1:50-1:58; 3:50-4:15; 5:00-5:07; 6:25-6:30

 

 

Thanks and Regards,

Aditya Kulkarni

3 REPLIES 3

Re: Unplanned % in statistics indicating wrong value

Please find attahched the shift table as it is not properly visble above.

Re: Unplanned % in statistics indicating wrong value

Genius
Genius

Hello Aditya,

 

You have to eliminate the starting time from 0 hours to 6.50 hours in the simulation, then you will get 12.82%. Statistics will consider the data from time 0 by default. To avoid that please enter the time from what time the statistics data to be considered in the event controller, statistics tab.

 

Go to Event controller > Statistics - 6:30:00

Event controller > End time - 39:06:30:00

 

Thanks & Best Regards,

Abhilash S.

Thanks & Best Regards,
Abhilash Sridhar
Mercedes Benz R&D India, Daimler AG

Re: Unplanned % in statistics indicating wrong value

Thanks Abhilash its working