Cancel
Showing results for 
Search instead for 
Did you mean: 

Urgent! Program crash, need urgent help opening model.

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello,

 

I am running Plant Simulation V12.1 of a model with 3D data. Upon saving the model as usual yesterday and shutting off my computer, my model will not open today. It says there is invalid 3D data and that the 3D data will be created from scratch. Upon accepting this dialog, Plant Simulation hard crashes with no backup file. My other backup files of this model present the same problem, so I have no backups to go back to.

 

Is there a way to force Plant Simulation to open a model without loading 3D data by using command line parameters?

 

The error messages are attached.

 

Thank you.

2 REPLIES

Re: Urgent! Program crash, need urgent help opening model.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

as it seems the 3D part in your model is corrupt.

 

To analyse this further we need the model file.

 

If you cannot post it here in the forum please open a GTAC call.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Urgent! Program crash, need urgent help opening model.

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello,

 

Thank you for your reply. A GTAC call will be opened by one of my solution partner colleagues.