Cancel
Showing results for 
Search instead for 
Did you mean: 

User-defined ribbon tab method call with parameters

Legend
Legend

Hello,

 

I have problems with calling methods in 12.2 from the user-defined ribbon tab. When specifying a method to run when clicking an item in the user-defined ribbon tab, the method starts but it says that the list-parameter is unidentifiable even though it should be a list with the SingleProc that the frame contains. This works in 12.1 but not in 12.2. I've also gotten crashes while testing this especially when trying to use the new default arguments to the method.

 

unidentifiable.PNG

1 REPLY 1

Re: User-defined ribbon tab method call with parameters

Siemens Phenom Siemens Phenom
Siemens Phenom

Thank you for reporting this bug. It will be fixed in the next patch for version 12.2.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.