Cancel
Showing results for 
Search instead for 
Did you mean: 

User interface concept in Plant Simulation 11 TR1

Legend
Legend

Hello everyone,

 

In TR1, the user interface concept was added under Tools -> Preferences -> User Interface. For me, this option is locked to Menus and Toolbars, how do I change this?

 

Running Windows 7 64-bits with the 64-bit edition of Plant Simulation 11 TR1.

3 REPLIES 3

Re: User interface concept in Plant Simulation 11 TR1

Siemens Phenom Siemens Phenom
Siemens Phenom

This feature will only be available in Plant Simulation 11 TR2.

 

So you can ignore this setting in TR1.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: User interface concept in Plant Simulation 11 TR1

Legend
Legend

Thank you Ralf,

That was not obvious from the help text.

 

As a side note, what does TR stand for?

Re: User interface concept in Plant Simulation 11 TR1

Siemens Phenom Siemens Phenom
Siemens Phenom

It stands for Technological Release. Basically it's a fast way to get our customer early access to new features between our major releases.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.