Cancel
Showing results for 
Search instead for 
Did you mean: 

Using a nested table in the experiment manager input parameter

Pioneer
Pioneer

When I try to give the cell of a nested table (2 level) as an input parameter in the experiment manager then I get an error. Is this not supported, or am I doing something wrong?

 

Thanks in advance.

2 REPLIES 2
Highlighted

Re: Using a nested table in the experiment manager input parameter

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi!

Works fine in my model. What is the error? Probably it's easier to share the model.

Here's a screenshot with all relevant windows:

ExpManager_NestedTable.png

Regards, Vladimir.

Re: Using a nested table in the experiment manager input parameter

Pioneer
Pioneer

Thanks, there must have been a typo that I didnt identify.