Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

V.13 does not provide the auto complete "is do end;" when a new method is created?

Builder
Builder
I am testing the v.13 and I noticed that the auto complete "is do end;" when a new method is created is not being performed anymore. Was this due to some improvement?
1 REPLY 1

Re: V.13 does not provide the auto complete "is do end;" when a new method is created?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
by default the method are with the new syntax of SimTalk, so you don't need is,do,end (see help)
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net