Cancel
Showing results for 
Search instead for 
Did you mean: 

VSM Process_assmebly settings

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello GG,

         Can you tell me how to set parameter of  by a method?

         I know there are two tables, Products, SubParts, but I don't know how to link them, which is different with Process object.  see the domo model in the attachment.

        Thanks very much!

         

1 REPLY 1

Re: VSM Process_assmebly settings

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello dongshui8558,

 

The object Process_Assembly has two different tables to define the product and the bill of materiel.

First the product is defined in table Product_Tab with the columns: Product, Lotsize, Cycletime, Transfer rate, Rework rate and  Scrap rate

The second table defines the bill of material and is called PartsList. It ha s the columns Base , product, Quantity and Used in Product.

 

Hope this will help you.

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution