Cancel
Showing results for 
Search instead for 
Did you mean: 

Version conflict with OPC

Experimenter
Experimenter

Hello,

 

at the moment i try to connect PlantSim and an OPC server for testing. For this purpose i use the build in OPCInterface, but i don't get a connection. (CoCreateInstance: Class not registered error)

According to the help it is only possible to connect them when they have both 32 or 64bit.

I guess the problem is, i have access to PlantSim v12 64bit and v13. All the servers i have tested are 32bit.

 

So with the v13 it's not possible anymore to connect to a 32bit server, cause it is only delivered in 64bit?

Is there a workaround for this problem?

 

Or is there a (free) 64bit OPC Server alternative, where the connection works?

 

Thanks and Greetings,

2 REPLIES 2
Highlighted

Re: Version conflict with OPC

Siemens Phenom Siemens Phenom
Siemens Phenom

You should be able to connect to a 32-bit OPC server, if it is an OPC classic server (OLE for Process Control) and not an OPC UA server (Unified Architecture). OPC UA is not yet supported. It will be supported in Plant Simulation 13.1.

Did you install the OPC Core Components for 64-bit? You can find the installation package "OPC Core Components Redistributable (x64).msi" in the folder "OPC Data Access 3.00 Core Components" in the downloadable zip file that contains the setup for Plant Simulation.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Version conflict with OPC

Experimenter
Experimenter

Hello,

 

the Core Components were missing. I haven't looked into the zip file, so i haven't seen them. Thanks a lot!

 

Greetings