Cancel
Showing results for 
Search instead for 
Did you mean: 

Vessel displaying the level of its content through a display panel.

Master
Master

Hi all,

 

We built a vessel, and added a display panel which is used to display the level of fluid in the Vessel. But, unfortunately, the display panel wasn't showing th level of fluid content in the vessel. We have attached the 3D model of the vessel which has the display panel as well. Could anyone help us out regarding the same?

 

Thank you

1 REPLY 1
Highlighted

Re: Vessel displaying the level of its content through a display panel.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello sahana_s,

 

did you use a tank of the Fluids Library to model your vessel? If that's the case you would have to reference the attribute CurrentFillLevel of the tank object in the path of the display. I have attached a model where that worked for me, it contains a tank and a display showing the current fill level of it.

 

Kind regards,

 

Igor Kunjavskij

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution