11-17-2015 03:07 AM
A - let's say "interesting" behaviour can be observed in PlantSimulation 12.
I have formatted a table row as real with a formatting of -15.14, meaning 14 digits behind the comma are required.
If I enter 33.33333333333333 or 33.33333333333334 manually PlantSimulation 12 immediately reports an error?!?
Wehn I enter a formula as =100/3, everything is more or less all right. The result is rounded wrongly (but correctly exported to excel).
At least Siemens has learned from the fromer error reports and is not allowing any more to upload a demo model for reproducing. Very helpful!
11-17-2015 07:18 AM
Hi Mak,
your numbers have 16 digits and your format defines a maximum of 15.
This is the reason for the error.
I'll check why it's currently not possible to upload a model.