Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

What is and How i can use it? - Recovery Time

Hi guys,

So i Want to know What is and How i can use The Recovery variable, cause it dont even counts in the sheets and in the statistics, but it does change a lot of stuffs in the others statistics.

-thanks

12 REPLIES 12

Re: What is and How i can use it? - Recovery Time

Phenom
Phenom

What do you mean by recovery variable ?

 

recoveryTimeMode ?

Re: What is and How i can use it? - Recovery Time

no...how can i explain.. just the Recovery time that you can put in the Single Proc Control Panel, what does he do, mean and change in the simulation; and how can i use him (if you can give me an example i will help a lot)

Re: What is and How i can use it? - Recovery Time

Phenom
Phenom

For an explanation / example, have a look here, in the help file:

 

Unbenannt.PNG

 

 

Re: What is and How i can use it? - Recovery Time

i've looked in the help file, but it didnt help kk this just made me more confused about it

Re: What is and How i can use it? - Recovery Time

And i looked here and my simulation with ou the recovery time ends at day 18 and with the recovery ends at day 12, thats why i have to understand the recovery thing to explain why the end date have this 6 days difference.

Re: What is and How i can use it? - Recovery Time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

the default behavior is as follows: if a MU exited the station, the next can enter without delay.

Now there are many cases, where this is different, e.g. you need to clean the machine, before the next part can enter or the part cannot leave, because you need to evacuate the mist inside the machine or the parts need to cool down... however, you need in this cases a defined waiting time; this you set with the recovery time; statistically it is waiting time for the station; it increases the dwell-time of the parts

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: What is and How i can use it? - Recovery Time

So this "cleaning" improves the efficiency of the Stations?

Re: What is and How i can use it? - Recovery Time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

depend on, how you define cleaning

if you define cleaning as non-productive time, then it reduces the efficiency...

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: What is and How i can use it? - Recovery Time

i have this model and when i run it with the recovery it changes the day that it ends, like this.:
1 (after the part enter) - it ends at 29/05/2019.
2 (after the part exit) - it ends at 31/05/2019.
3 (after the process ends) - it ends at 27/05/2019
and at last but not least the 4 one that i removed the Recovery from the control panel and it had ended at 31/05/2019.
Why this 4 trys had a different end date?