Cancel
Showing results for 
Search instead for 
Did you mean: 

Where a method is already use ?

Creator
Creator

Dear,

 

I'm currently learning the software Plant Simulation and I have a very simple question.

 

1/ I create a method.

2/ I use it in several objects

 

If i don't remeber where I have used it, does-it exist a table to show me that this method is used in these objects ?

 

Thanks for your response,

 

3 REPLIES

Re: Where a method is already use ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Jer_N,

 

unfortunately there is no such table.

 

But you could use the find command which is in the context menu of the class library objects.

Here you can search the program text for certain method names.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Where a method is already use ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Note: If you want to use "Find Object..." to find all locations where the Method is used, you need to select "Attribute" in the drop-down list box. This way you will not only find all Methods that call your Method, but also all object that use your Method as a control.

 

The setting "Attribute" means that Plant Simulation searches the search string in all attributes, including the attribute "Program" of Methods, which contains the source code of a Method, and the attributes for controls like "ExitCtrl", "EntranceCtrl", "PullCtrl", ...

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Where a method is already use ?

Creator
Creator

Thanks a lot !