Cancel
Showing results for 
Search instead for 
Did you mean: 

Worker Based Upon MU Attribute

Creator
Creator

I have a station that process two products.  In the model, I differentiate these products with a boolean attribute.  MUs with an attribute value of "true" will require the station to import a worker for the cycle.  For MUs with an attribute value of "false", will not need a worker to cycle.   How can I call a worker for some MUs with a "true" attribute, and not call a worker for MUs with a "false" attribute?

1 REPLY 1

Re: Worker Based Upon MU Attribute

Phenom
Phenom

Hi @SIMmer_Down 

 

You can use the MU Name to do that. If you are using PlantSim v14, it is possible to use the parameter ImporterActive. If you are using PlantSim v15, take a look at the attribute imp.Active.

 

Anyway, take a look at the model attached, specially in the Entrance Control of the Station.

Best Regards,
Paulo Araujo

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.