Cancel
Showing results for 
Search instead for 
Did you mean: 

Worker problem

Builder
Builder

hi everyone,

 

i have a situation where i have 4 manual workstations(single proc) with 1 worker assigned to each   station.problem is that each worker has to carry a part from source,go to that single proc ,work there and then carry the part to the drain.my problem is that how to fix the position of workers so that worker 1 go to place 1 ,worker 2 at place 2 and so on. Need some help!!!

4 REPLIES

Re: Worker problem

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi k_parashar,

 

if you have such a clear assignment you can use for each set of stations a different WorkerPool and Broker which has just one worker.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Worker problem

Builder
Builder

hi Ralf,

 

Thanks for the help,but i have to send the parts to the station which is free out of the 4 station.i am using buffer to store the parts and then the workers carry the parts to the respective workstation.but the problem is i can assign only one MU target in the carry part away of the buffer .How can i assign the target in the buffer?

Re: Worker problem

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi k_parashar,

 

This would be the simplest with a little SimTalk. You should assign each workstation a unique service and have one worker for each service. In the Source you need an entrance control that selects the workstation, then you set that as the required service to carry the part.

 

Regards,

Gert Nomden


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: Worker problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi k_parashar,

 

the destination for the carry-operation you set with <object>.MUTarget.

To get the right worker, you need to change the service table of the transport importer:

<object>.transportImp.setServices

 

You can use the exit control of the buffer to wait for an available machine and make the settings.

With @.move the worker is called.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net