Cancel
Showing results for 
Search instead for 
Did you mean: 

Worker to follow a specific listed order to move parts

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi all

 

On my model I have sub-assembly parts on different stations which has to be moved to the main assembly station. Please take a note that each sub-assembly station has its own source feeding it. So I want to use one worker to carry one sub-assembly part at a time and drop it to the main assembly, however I am struglling with telling the worker to pick the sub-assemly parts, following a specific listed order when picking parts from sub-assembly stations to the main assembly station. Which method can I follow? (This is a job shop manufacturing process actually)

 

Thank you in advance.

7 REPLIES 7

Re: Worker to follow a specific listed order to move parts

Hi Mosibudi_R,

 

did you have look at the collection of little sample models in Plant Simulation?

The one in my Screenshot is, I guess, quite close to your problem.

 

Andreas

 

WorkerExample.PNG

Highlighted

Re: Worker to follow a specific listed order to move parts

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I did see this one but the thing is in my case, each station has its own source.

Re: Worker to follow a specific listed order to move parts

Yes, but the point of the sample model is, that the worker has a fixed sequence of stations where he works and that also applies to your problem, if I understood you right: 

  1. bring parts from source1/station1
  2. bring parts from source2/station2
  3. ...
  4. start from the beginning. 

Re: Worker to follow a specific listed order to move parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

if you set the attribute: automaticMediation of the worker to false, you can send the worker with the command goTo to the next workplace, there you can place an entrance control to program the action of the worker (e.g. adress a MU and load it). You need to set the attribute destination of the MUs, if you want to carry them.

At the assembly station the worker unloads its parts automatically (you need only to wait, until he is empty).

So, you can program very easily a sequence of tasks.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Worker to follow a specific listed order to move parts

Creator
Creator

@Steffen_B Where did you set the attribute automaticMediation to false in your model? The method with goTo is pretty straightforward, but we can't find the modified attribute.

Re: Worker to follow a specific listed order to move parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I changed it directly in the worker class in the class library (F8...)

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Worker to follow a specific listed order to move parts

Creator
Creator

Found it! Thank you!