Cancel
Showing results for 
Search instead for 
Did you mean: 

Worker transport and directly processing

Creator
Creator

Hello community,

 

 

I have one worker with a capacity of 5 MUs. He should take 5 MUs from a left side buffer and transport them to one of the right side buffers. After each transport he should immidiately work on the 5 MUs on the singleproc behind. After working on the 5 MUs he should go back and repeat the whole circle with the next 5 MUs. (The important part for me is how to control the worker to go, stay and work at the singleproc for 5 MUs)

 

Could someone please tell me how i could do that. I had some tries with the request control in the Broker but it didnt work. 

 

2018-07-03 16_32_47-Clipboard.png

 

 

1 REPLY

Re: Worker transport and directly processing

Creator
Creator

 

Solved:

I have just added a Release Control to the SingleProcs and i set up the priority of the Singleprocs to 1 (or higher). 

 

Release Control:

 

if Puffer4.leer = true and ?.belegt = false

 

?.imp.gebeExporterFrei

end