Cancel
Showing results for 
Search instead for 
Did you mean: 

Worker walking into Plant Simulation

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi All,

 

See the attached file for a simulation considering a worker walking animation. Sometimes it could be interesting for presentations. Smiley Happy

 

 

(view in My Videos)

 

Best Regards,
Paulo Araujo
12 REPLIES 12

Re: Worker walking into Plant Simulation

Valued Contributor
Valued Contributor

Considering posting a short video of the simulation run. That way people who don't have Plant Simulation can just use the video in their presentation. It looks good. Thanks.

Re: Worker walking into Plant Simulation

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Good point Abhijit, The short video is attached as a zip file.

 

All, take version 2 of the simulation, now there is a waiting pose.

Best Regards,
Paulo Araujo

Re: Worker walking into Plant Simulation

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

To watch the video you will need the Camtasia codec (attached).

Best Regards,
Paulo Araujo

Re: Worker walking into Plant Simulation

Valued Contributor
Valued Contributor

I have embedded your video in the post itself. You can embed mp4 videos in your post in the community

Re: Worker walking into Plant Simulation

Pioneer
Pioneer

Hi Paulo,

 

this is awesome, thanks for sharing this walking worker with the nice graphics with us! I have exported your object to make it usable in all my models.

Kind regards

M.

Re: Worker walking into Plant Simulation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Paulo,

 

This look awesome!!

 

If Plant Simulation would allow self animations for MUs we could create some amazing stuff!

 

Gert Nomden


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: Worker walking into Plant Simulation

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Using a little trick, you actually can do that.

Although it is impossible to create self animations directly on MUs you can create a viewer object on an MU. (I would suggest to do so in the class).

Such viewer objects are capable of self animations as every "normal" object (e.g. a SingleProc) is.

 

To create a viewer object in an MU that represents the entire MU, select the graphic of the MU and call "Make Viewer Object" from that graphic's context menu.
If there is no single graphic that represents the entire MU, you might want to group the graphics first.
If a nested MU (e.g. an Entity on a Transporter) shall be affected by the self animations you add to the "main MU" this way, you will want to forward this nested MU. To do so, you have to write some code in SimTalk:
Assume, t is the transporter that carries the entity and the self animating inner viewer object is named "Content". The SimTalk code "t._3D.AnimationObject := "Content"; " will configure the transporter (and its derivates) to forward every MU that enters the transporter to its nested viewer object "Content".
Now you have to add the needed animation paths to the nested viewer object (e.g. by copying via tables) and the Entity will follow every move of "Content"'s self animation.

Re: Worker walking into Plant Simulation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi Peter,

 

We ran some tests, but it is not really obvious to get it running properly. I suspect that the current state of Plant does not allow a simple kinematic model of e.g. a walking human. One just needs a small kinematic chain, graphics and some simple rotations. All this stuff is available within Siemens! Maybe something for development to look at...

 

Thanks for you support anyway!

 

Gert


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: Worker walking into Plant Simulation

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Actually, with some preparations, this is possible (if you can split your desired animation in several animating parts). As long as you don't want to model ball joints (which is possible but somewhat more difficult since the rotation axis would have to be redefined continuously), you can define arbitrary rotation (or other) animations:
Assume o is the object you want to animate. A simple joint has a fixed rotation axis so it is sufficient to define that axis once in the 3D properties dialog for this object - the rotation axis is found in the middle of the "Transformation" property page. Now you can plan arbitrary combinations and sequences of animations for that object and play them. In the case of a joint this is a pure rotation which can be planned with

o._3D.SelfAnimations.scheduleRotation(<startAngle>, <targetAngle>, <angleVelocity>);

If o is a pure viewer object with name "x", e.g. directly nested in the object p, this would be
p._3D.getObject("x").SelfAnimations.scheduleRotation(<startAngle>, <targetAngle>, <angleVelocity>); instead.
E.g. to rotate the base of the robot <r> from 0° to 180° with 90°/s, this would be r._3D.SelfAnimations.scheduleRotation(0, 180, 90);
The subsequent call
r._3D.SelfAnimations.playAnimation;
now starts the animation.
Base upon that pattern, it is possible to model quite complex animations.

Note that the time source for these animations is the event controller if a simulation is running and the CPU time otherwise.
To react on failures in your machine, you can pause your animation with
o._3D.SelfAnimations.pauseAnimation;