Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Worker walking into Plant Simulation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Check!!! With your help it works (did not access the embedded viewer objects properly).

 

If this can be realized without SimTalk I would call it a winner!


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: Worker walking into Plant Simulation

Phenom
Phenom

Hi Nomden,

 

just to proove that kinematic chains, graphics and some simple rotations are definitely no issue in V11 and to underline, what Peter Komarek stated, I've added a tiny hexapod example.

 

The geometric core is based on the hexapod robot from Tim Mills.

 

The kinematics/animations  are 100% V11

 

hexapod.JPG

 

Re: Worker walking into Plant Simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

Thank you simulator. The animation is great.

 

Unfortunately, Plant Simulation 11.0.0 to 11.0.4 has a bug that sometimes prevents exchanging a model between the 32-bit and the 64-bit version of Plant Simulation. Your model 'hex88.spp' is such a model. The bug is fixed in 11.0.5, which is not yet released. I loaded the model into a preliminary 11.0.5 64-bit version and saved it as 'hex88_64bit.spp', so that you can load it into a 64-bit version of Plant Simulation 11.0.4.

 

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.