Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Workers assignement

Pioneer
Pioneer

Hi,

I created a model with 2 work stations on 2 SingleProc and exit strategy "carry part away" (with worker pool and the broker).

If I set the process time as "costant", the system use both the workers, if I set: process time -> List(type), only one worker work and the other one rest in the worker pool.

 

Thanks

2 REPLIES 2

Re: Workers assignement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

have a look in the statistics of the workers. The workers are waiting almost the complete time. If you have the same times, than you need two worker at the same time (if the machines run sychronous). If you change the times with your table, the machines calls the worker one after another. The broker mediates every time the first available (every time the same).

Nothing wrong with your model.

 

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Workers assignement

Pioneer
Pioneer

Thanks!