Cancel
Showing results for 
Search instead for 
Did you mean: 

Working with Source part sequences

Pioneer
Pioneer

I'm trying to find a way to modify which part of the sequence is supposed to be processed

 

ideally the sequnce in the datable is how i want the parts to be produced. But when there is overstock that occurs once in a while for that part, I need the source to jump to the next part or the part with the lowest inventory level. I am just trying to figure out how to get code into the datatable-source system.

 

Thanks

4 REPLIES 4

Re: Working with Source part sequences

Phenom
Phenom
Will your stock pull the parts always?
Best Regards,
Paulo Araujo

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Working with Source part sequences

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi  Haseeb,

 

it is possible to change dynamically the SequenceTable. Please see the attached model for Plant Simulation 14.0.

To verify you can use the creation table of the Source object, see tab Statistics.

 

Regards,

Peter

Re: Working with Source part sequences

Pioneer
Pioneer

Yes It will. The Downstream processes from the inventories operate at different schedules. I just need to see if I can jump from a part in the sequence to next if one inventory is currently full

Re: Working with Source part sequences

Pioneer
Pioneer

Is there a way to rearrange the row orders based on their attributes? I dont want to rewrite the table necessarily