Cancel
Showing results for 
Search instead for 
Did you mean: 

Workstations with different station length

Hello Guys, I have a query in the model I am building now. I have 10 stations each having different station length. But in 3D view of my model, all Stations have same dimension. Is it possible to vary the 3D appearance of station as per required dimensions? Also is it possible to overlay AutoCAD 2D and precisely build model on the same?
3 REPLIES 3

Re: Workstations with different station length

Phenom
Phenom

yes, you can.

e.g. through scaling in 3d  ( select 3d object and press cntrl 3)

 

 

@ autocad

drag & drop layout on 3d window

or create a textured plate with the dwg contents ( jpg/png.. format)

 

for details s. help

 

 

 

Re: Workstations with different station length

Another doubt - Distance between 2 points in the Grid in 3D is 1m - Am I correct?

Re: Workstations with different station length

Legend
Legend

It is by default 1m but it does not necessarily have to be 1m. By default it shows 3 types of grid lines as follows. But they can also be changed by double-clicking on the cell.

 

Here:

Unbenannt.PNG

 

Sanchay