Cancel
Showing results for 
Search instead for 
Did you mean: 

an Error of changing the capacity of transporter?

Genius
Genius

Hello,everyone

 

There is an error  happenning when i  change the capacity of the transporter.

As is shown in the following picture:

Firstly, I wanna set the capacity  of the transporter "Pallet4" with marked 1:

Secondly, the settings are shown with marked 2.

X-dimension:11 (or  larger)   

Y-dimension:1

Z-dimension:1

After that,there something wrong with it,the results are shown  with the pop-up marked 3.

 

I have no ideas how to deal with it.

Looking forward to your directions.

Any help is great appreciated!

 

 

捕获.JPG

1 REPLY

Betreff: an Error of changing the capacity of transporter?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Mark Lee,

 

the error message tells you there is a MU on a place which you want to reduce.

If you want to reduce the capacity of an object, the object must be empty. Otherwise you may get this error message.

 

Hope this helps.

 

Regards

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution