Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

assembly station exit

Hi,
I would like to have an information about the assembly station exit strategy.
In my model I have a Main MU that has to contain two different entities one at a time. When the two entities arrive in the assembly station I have to send the Main MU in two different lines depending on which of the two entities is contained. If the Main MU contains entity1 it has to go to line1, if the Main MU contains entity2 it has to go to line 2.
I hope someone could help me.
Thank you very much for your time.
Marco

2 REPLIES 2

Re: assembly station exit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

i guess, there is no prepared exit strategy for your case. But you could use a exit control (rear) to distribute the parts. With @.cont you can access the assembled part and using the name you can create a decision:

 

if @.cont.name = "entity1" then

  @.move(line1);

else

  @.move(line2);

end;

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: assembly station exit

Wow great! It works perfectly!
Thank you Steffen, you are always very helpful!
Best regards.
Marco