Showing results for 
Search instead for 
Did you mean: 

automatically pop up Edit 3D properties of Frame object

Valued Contributor
Valued Contributor

Hello All,


I  would like to know the way of automatically pop up "Edit 3D propoerties" of Frame object by coding.

I am developing user interface using dialog object for 3D simulation modeling.

A point cloud file is able to load into Frame in 3D model,but I have to click the edit 3D properties by manual to adjust (size, x,y,z, coordination) imported point cloud.  Instead of clicking the  mouse right, I would like to add coding in dialog for an automaic pop up.

I appreciate your comments. :-)




Re: automatically pop up Edit 3D properties of Frame object

Siemens Phenom Siemens Phenom
Siemens Phenom

I'm sorry but there is no function to open a 3D properties dialog.

However, you can set the position and rotation of a point cloud via SimTalk with the attributes _3D.PointCloudPosition and _3D.PointCloudRotationAngle.

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution