Cancel
Showing results for 
Search instead for 
Did you mean: 

average processing time and average time of arrival for a resource

Experimenter
Experimenter

I want to calculate the average time processing for a machine and the average time between two arrival. Can someone help me? 

2 REPLIES 2

Betreff: average processing time and average time of arrival for a resource

Siemens Phenom Siemens Phenom
Siemens Phenom

Open the statistics report for the station. Check the detailed "Working Time" line. The "Mean Value" is what you are looking for.

The "Wainting Time" line shows the other value in the "Mean Value" field.

Re: average processing time and average time of arrival for a resource

Phenom
Phenom

Average processing time = average cycle time can

 

be calculated through the delta time between

 

2 MU exits

 

If you store the delta time(s) in a table,

 

the table.meanvalue - method calculates the value for you.

 

@ delta time

store the exit time in a (global) variable

 

and subtract the variable from the exit time

 

of the following MU through an station exit method

 

For mean arrival(s) it's the same procedure but using the entry method

 

IF the arrival frequency is higher than the exit frequency you should set

 

a buffer with a high capacity before the station and measure the arrival time at the buffer entry