Cancel
Showing results for 
Search instead for 
Did you mean: 

bug with a methCall in ShiftCalendar

Legend
Legend

Hello,

 

I want to use a self.methCall on an user-defined method in a ShiftCalendar.

 

I can see the methCall in the event debugger but when it is "Called", it is not executed.

 

Attached a model with the same bug. I use plantsimulation 13.0.0

Is it a bug ? Or a mistake ?

 

best regards

2 REPLIES

Re: bug with a methCall in ShiftCalendar

Siemens Phenom Siemens Phenom
Siemens Phenom

This is a bug. Smiley Sad

It will be fixed in the next version.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: bug with a methCall in ShiftCalendar

Legend
Legend
OK, good to know.