Cancel
Showing results for 
Search instead for 
Did you mean: 

class hierarchy/tree

Valued Contributor
Valued Contributor

Hi,

 

im looking for an overview from all classes. Something like a tree or object model where I can see how the objects in Plant Sim inherit. The Help (F1) is a bit confusing because there are not all Attribute listet and some that are listed in the help are not inherit by the objects ...

1 REPLY 1

Re: class hierarchy/tree

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Readock,

 

there is no inheritance between our standard objects.

To view all the attributes an object has it's best to use the context menu of an object and select 'Show Attributes and Methods".

 

This gives you all the attributes and methods and you can use the toolbar to limit the the scope to a certain area.

You can also press the F1 key when you have an attribute or method selected to jump to the online help.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.