Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

container loading

Creator
Creator

Hi everyone

I am just new to this software and I has a quetion about container.In short, my production situation is that there is a machine one(M1).Every part produced by M1 go to the containers(there are 2 containers) which are just next to it for temporary storage and after M1 produces 100parts, the container 1 is full and is tranported to M2. Meanwhile, a empty container next to M2 is tranported back to M1.

 I tried to use container and it seems it doesnt load and go to buffer then it disapper. How can I deal with this?

 

Kind regards

 

8 REPLIES 8

Re: container loading

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

look at this example:

 

http://www.bangsow.de/detail_en.php?id=304

 

Look into the exit controls of the container-place and machine.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: container loading

Creator
Creator
Thanks for answering. But it is strange that I can not open this link of the sample. It will be really grateful of you if it is possible for you to attach the sample here or send me privately by e-mail?

Re: container loading

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

it is a problem with the internet-explorer. there are some computer-virus types with the extension .spp, so the download will be changed to a text/html-file. But if you right click on the link and select target save as --> change the file extension to .spp, this should work.

 

But you also find the file attached.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: container loading

Creator
Creator

Thanks,I got it and in this case, it is able to solve my original problem.But when I add a parallel machine(M11) with M1, the material flow isnt distributed with the setting of the Exit strategy which I set up of previous machine(M0). All part only go to M1. How can I solve it? 

Re: container loading

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

if you want to load two machines from one box, you need to change the exit-control of the entrance-place. Just add a line for the second machine. The exit control of the machines then pulls the parts from the box. Perhaps you need also extend the exit control of the machines to avoid an access to an empty place (if one machine has moved the empty box ).

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: container loading

Creator
Creator

Now it is no problem with flow distribution but a new problem of parts transporting comes.Probably you can look a bit into it? I think I need to change sth in the Method but I dont know how. 

Re: container loading

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

First: i would recommend only to use one finished part place, so that you can finish containers (only P2) . The second machine can find a empty place. Try this as LoadProcess:

is
do
   --load the part into the pallet
  @.move(?.bufferReadyParts.cont);

  if ?.bufferReadyParts.cont.full then

    --move full pallet to successor

    ?.bufferReadyParts.cont.move(?.successor);

  end;

 

  if ?.bufferGreenParts.occupied then-- may be empty

    ?.bufferGreenParts.cont.cont.move(?);

    if ?.bufferGreenParts.cont.empty then

      --move empty pallet to ?.readyparts

     ?.bufferGreenParts.cont.move(?.bufferReadyParts);

     --create new pallet

     createPallet(.MUs.pallet,.MUs.part,M0);

   end;

end; 
end;

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: container loading

Creator
Creator

Thanks for all of your suggestions and it works perfectly.