Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

content of a buffer

Pioneer
Pioneer

Hello,

 

I want to write the content of a buffer in a list. So I need a code to give back an integer. 

 

The problem is that the code buffer.inhalt gives back an object. 

The code buffer.capacity only gives back the whole capacity. 

 

But I need to write the number of MUs that are in the buffer in that moment. Is there an option for that?

2 REPLIES 2

Re: content of a buffer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

it is

 

numMu

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: content of a buffer

Pioneer
Pioneer

Thank you!!