Cancel
Showing results for 
Search instead for 
Did you mean: 

creating a dual Lift bed

Pioneer
Pioneer

Hello Everyone

 

the problem i having right now is.

a dual line system where both levels run at the same speed and have the same number of parts in them.

 

it then comes to a lift section that need to load from the last line, then they both move up at the same time and speed to a set position. and then when bot lines have emptied the lift then moves back down to the rest position which is also the load position,

these lines need to move in a forward and a backwards way and they are a feed-in and feed-out of the system.

 

any help with this system would be great i have a plan of doing the system as a line then moving the lines up at the same time in the 3d world.

 

Thanks

Gareth

10 REPLIES 10

Re: creating a dual Lift bed

Phenom
Phenom

do you mean something similiar to this ?

(view in My Videos)

Re: creating a dual Lift bed

Pioneer
Pioneer

Hello Simulator

 

this is close to what i am looking for but there would be two lift beds one above the other they will then be feed by two lines then feed off to two lines,

in the same way that yours feeds off no.

 

Thank you for the video this help me understand that it is possible.

 

but it is not quite what i am looking for

 

Gareth

Re: creating a dual Lift bed

Experimenter
Experimenter

Hallo simulator,

I need exactly this function. Can you send me your model?
I tried to model it with a conveyor and an vertical animation line. The problem is that the conveyor has to move backwards at the lower floor.

Regards Peter

Re: creating a dual Lift bed

Phenom
Phenom

Hello Peter,

 

as I have no access to the uploaded videos -are you

 

refering to this model /video ?

 

3Gduepif0T1UGY8H4xMDoxOmdsOy-VNr.jpg

Re: creating a dual Lift bed

Experimenter
Experimenter

Yes exactly. Do You have the model?

Re: creating a dual Lift bed

Phenom
Phenom

Yes, the model should be available.

 

Concerning the elevator there have been some updates to improve flexibility.

 

I will see what I can do to provide.

 

Might take a day or two.

Re: creating a dual Lift bed

Experimenter
Experimenter

Thank You, that´s great!

Re: creating a dual Lift bed

Experimenter
Experimenter

Hi simulator
Did You found the model? 

Re: creating a dual Lift bed

Phenom
Phenom

Peter,

 

please have a look

Unbenannt.PNG