Cancel
Showing results for 
Search instead for 
Did you mean: 

defect object error

Pioneer
Pioneer

i have created to object that are processed at a machine. the defective products that are generated are 0.7 for b and 0.2 for a

 

the model show error when i try to run, as it doesnot identifies the attribute for object Unbenannt.JPGa

1 REPLY

Re: defect object error

Phenom
Phenom

Hello.

 

Inside the MU called 'b' there is no attribute called 'quality_a' but instead it is called 'quality' instead.

 

If both of them are meant to have the same function in both MU's then I would recomend using the same name to make your code more simple.

 

JamesM