Cancel
Showing results for 
Search instead for 
Did you mean: 

define sequence in source

Pioneer
Pioneer

Hi

 

I want to model a plant in which the source should produce 2 no.s of variant a and then 1 no. of variant b.

In class library I have defined the 2 MU's as variant a and variant b.

 

Further 2 cases can arise

1)when no.s of the 2 variants are not limited and keep on producing in ratio 2:1

2) when no.s are limited like 1200 cars of variant a and 600 cars of variants b

 

Please inform how to go about it

 

2 REPLIES

Re: define sequence in source

Genius
Genius

Hello Aagosh,

 

please find the model attached

Thanks & Best Regards,
Abhilash Sridhar
Mercedes Benz R&D India, Daimler AG

Re: define sequence in source

Pioneer
Pioneer

Thanks a lot Abhilash......Accepted as solution! It was easy i should have done it