Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: disassembly via Method, generating MUs with user attributes

Phenom
Phenom

@ assembly / dismantle

 

have a look

 

 

Unbenannt.PNG

Re: disassembly via Method, generating MUs with user attributes

Valued Contributor
Valued Contributor

Thank you for the example. unfortunately, I am working with version 11, so I cant open.
And if I do as you suggested, the problem is that both MUs are not conveyors but regular movable units;
so I get this notification:
1.PNG
I am currently building towards a solution to place all the assembled MUs in a buffer; (sorting them out specifically)
delete them there and create the 2 components via a method in the entry control.

Re: disassembly via Method, generating MUs with user attributes

Phenom
Phenom

if you exchange the Mus through a containers it will work.

 

Or you can set the assembly mode to "delete MUs"

 

Then you have to create/name the Mus you want to disassemble at the dismantle station.

 

For details s. help