Cancel
Showing results for 
Search instead for 
Did you mean: 

eM-Server Update - Operation fail

Creator
Creator

In Process Simulate (12.1.2), I have a problem with the data that is actually stored on the eM-Server: I have a project with many operation,When I update the data to e-Msever, the situation shown in the picture appears, even if only the update operation is selected. Note“the file is not following reason XML error ‘System call failed’.line number 308 .colume=621097。It shows that the update was successful, closing the study and reloading it, there is actually no update. The modified data before the update has been lost.However, I actually faced this problem in several projects and it is really annoying

 

Does anyone have any ideas on how to get all the actual information stored on the eM-Server? Are there some settings that I have to take a special look at?eM-Server Update - Operation fail.jpgeM-Server Update - Operation.png

1 REPLY 1

Re: eM-Server Update - Operation fail

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi MqPS2018,

this is the Plant Simulation forum.

I believe you better post this in the Tecnomatix Robotics or General Tecnomatix forum.

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution