Cancel
Showing results for 
Search instead for 
Did you mean: 

error after experiments

Creator
Creator

Hi there,

 

when my experiments with the manager come to an end, I get this error and the results can not be visualized.

Does anyone know what kind of error is this? (attachement)

 

Thx for your help!

 

Selim

12 REPLIES 12

Re: error after experiments

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Selim87,

 

looks like an implementation error in the Experiment Manager.

 

Can you please tell us which version of Plant Simulation and which version of the Experiment Manager you are using?

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: error after experiments

Creator
Creator

Hello,

 

I'm using Plant Simulation Version 12.0.0 (Professional Licence). Where can I find the version of the Expmanager?

 

Regards,

 

Selim

Re: error after experiments

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Selim87,

 

you can find it either in the Library Manager (Rightmost icon in the Home ribbon category).

 

Or if you right click on the library folder in the Tools folder and select "Edit Library Information".

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: error after experiments

Creator
Creator

the version of the experimentmanager is 12.0.0 too

Re: error after experiments

Siemens Phenom Siemens Phenom
Siemens Phenom

I think the problem is already fixed in the patch 1 for V12. So can you please install this patch and then updated your Experiment Manager to the most current version using the Library Manager?

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: error after experiments

Creator
Creator

Hello Ralf,

 

I just updated to V12.0.0.2. Few things are fixed, but I still get the error message of the attachements. So once again, when the experiments are done, I have this error message.

 

Regards,

Selim

Re: error after experiments

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Selim87,

 

it seems that a table in your Experiment Manager is in a wrong state.

 

Can you insert a method in the frame where you have your Experiment Manager and add the following code:

is
do    
    ExperimentManager.pValues.tmpTables.open;
end;

 In the table which is then shown you should delete all cells.

 

Then the error should hopefully be gone.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: error after experiments

Creator
Creator

Hi Ralf,

 

Thx a lot for your prompt help! now it's finally working Smiley Happy))

 

best regards,

Selim

Highlighted

Re: error after experiments

Creator
Creator

Hi Ralf,

 

I have to ask you one last question about this thema. I have in my Model 4 frames, witch I need to compare the results. With your solution of Method, it did work for the 1st frame, but for the three others, I still get the same error message. When I run the Method, I get this table (1 cell is red, please see attachements).

 

Do you have any idea about the problem?

 

regards,

Selim