Cancel
Showing results for 
Search instead for 
Did you mean: 

error when use ExperimentManager

Pioneer
Pioneer

ExperimentManager error.png

I want to use the ExperimentManager. But once I open the random numbers, An error shows up.

" ExperimentManager.setseed is beyond the list of demension "

 

what can be wrong with this syntax?  Did I miss something?

MaxOfSeedvalues := tab.max(`[1,1]..`[2,*]) + 1;

 

8 REPLIES 8

Re: error when use ExperimentManager

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You should indicate range with {}, e.g.:

tab.max({1,1}..{2,*})

I would guess that " '[a,b] " is from a distant past.

 


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: error when use ExperimentManager

Siemens Phenom Siemens Phenom
Siemens Phenom

The syntax is following an old style but this shouldn't be a problem.

 

You are using a very old version of the Experiment Manager. So I'd recommend to update the library to the latest version.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: error when use ExperimentManager

Pioneer
Pioneer

thank  you! I have solved it.

Re: error when use ExperimentManager

Pioneer
Pioneer
Thank you! But what does "from a distant past" mean? (sorry for my english)

Re: error when use ExperimentManager

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I meant to say that the {} have been in use for a long time and that the `[] construct has been out of use for many versions. So, "a distant past" means "a long time ago".

 

As it seems, it still works in V11TR1, but not in the latest version.

 


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: error when use ExperimentManager

Pioneer
Pioneer
I see, Thank you again for your response!

Re: error when use ExperimentManager

Pioneer
Pioneer

The error shows "" ExperimentManager.setseed is beyond the list of demension " . I think maybe there is something wrong with the random seed in the model.

Re: error when use ExperimentManager

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I suspect the table has just one column, whereas your range assumes two. You could set the range as follows: {1,*}, meaning column 1 completely. Or just skip the range completely, since there is only one column...

 

It is a bit of guessing, since you use an old version.


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com