Cancel
Showing results for 
Search instead for 
Did you mean: 

experiment manager issues

Pioneer
Pioneer

Hi all,

 

I have a simple model with a flowcontrol and three singleprocs. As an experiment I want to change the percentage to each singleproc. Now I am stuck how to define the percentage in the definition of experiments as a string. Do I have to state a string with {70,20,10} or [70,20,10]? Can someone have a look how to define the experiments such that I can run multiple experiments with different percentages?

 

Many thanks in advance,

 

Eelco

2 REPLIES 2

Re: experiment manager issues

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The distibution in the FlowControl is set with the method <flowControl>.setExitList.

So you cannot access directly the values for the individual successors. You could instead define 3 global variables (for the experiment manager) and set the exitlist via the Init - method.

Look in the example.

 

exp.png

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: experiment manager issues

Pioneer
Pioneer

Thanks a lot SteffenSmiley Happy The example made it all clear, it a very practicle solution.

 

Eelco